Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Which pins have Weak Keeper Circuit? And can it select Enable/Disable?

Latest Updated:09/28/2009

Question:

Which pins have Weak Keeper Circuit? And can it select Enable/Disable?

Answer:

Please refer Section 19.6 Usage Note in the hardware Manual. You can not select Enable/Disable. The weak keeper circuit is always Enable.
Suitable Products
SH7619