Which pins should I use referring to the Pin arrangement in manual?
Latest Updated:03/25/2009
Question:
There are multiple pins with the same name when referring to the Pin Arrangement in the hardware manual. What does this mean? Which pins should I use?
Answer:
Answer
Suitable Products
SH7065 |
SH7058 |
SH7055 |