Which timing will extend if RAS is set up during CAS BFO RAS refreshment?
Latest Updated:03/23/2009
Question:
If RAS assert cycles are set up during CAS BFO RAS refreshment, which timing will be extended?
Answer:
SH7065=>TRrw is extended.
Except the above => the timing of TRc is extended.
Suitable Products
SH7065 |