Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Will transmission of E-DMAC be stop after relaying manual pause frame?

Latest Updated:03/25/2009

Question:

Transmit operation of E-DMAC will be stopped after transmitting the manual pause frame?

Answer:

No, it won’t.

It is the transmit operation of device received PAUSE frame by the manual PAUSE frame transmitting.

If there is a transmit descriptor effective for transmit buffer, SH7618 continues the transmit operation.

Suitable Products
SH7619
SH7618