Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Is protection against latch up built into the Renesas SRAM device?

Latest Updated:03/16/2012

Question:

Is a protection circuit against latch-up built into the Renesas asynchronous SRAM  device?

Answer:

We take measures against latch-up at the design stage and the process development stage. And we check the endurance with actual devices before mass production.
The latch-up evaluation results are included in our reliability report. Please request it if you need it.
Suitable Products
Asynchronous SRAM