Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can the uPD6467 be used with a progressive video signal, too?

Latest Updated:08/01/2005

Question:

Can the uPD6467 be used with a progressive video signal, too?

Answer:

It can support both interlace and non-interlace (it does not distinguish fields).
The dot frequency used may exceed the recommended operating frequency range in the case of double-speed scanning.
(The uPD6467 can theoretically be used at around 15 MHz but evaluate thoroughly for practical use.)
Suitable Products
A/D Converters