Skip to main content
Renesas Electronics America - Knowledgebase

Flash Development Toolkit OS Compatibility

Last Updated: 06/27/2016


What Operating Systems are compatible with the Flash Download Toolkit? Does the Flash Download Toolkit run in the Linux environment?


The Flash Download Toolkit only operates on Windows based machines. Linux is not supported at this time.

Supported Operating Systems:
Windows® 10 (32- and 64-bit versions)
Windows® 8.1 (32- and 64-bit versions)
Windows® 7 (32- and 64-bit versions)

For the most current list & specific details, please refer to: