Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Downloading and installing the free 128K eval version Renesas RX toolchain for e2studio

Last Updated: 06/09/2015

How do I install the free 128k eval version Renesas RX toolchain for e2studio?

This tutorial covers:
- registering with MyRenesas and logging in (required for download)
- accessing the RX compiler landing page:
http://am.renesas.com/products/tools/coding_tools/c_compilers_assemblers/rx_compiler/
- downloading the latest Renesas RX compilers
- installing the compiler
- starting e2studio afterwards and showing the easy Automatic Toolchain Detection feature (Installed RX and KPIT GNU toolchains (after v11.0x) are automatically detected and installed for use in e2studio when the product is launched).