Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Option Byte Configuration Recovery

Last Updated: 06/25/2016

Question:

How can I recover from a failed RL78 MCU programming process? What could be the cause?

Answer:

The video below demonstrates the the issue, explains a possible cause and how to use the Renesas Flash Programmer to recover your hardware in the event of a misconfiguration of the options bytes or lost security key.

 

http://www.youtube.com/watch?feature...&v=tISGgj2hh0Y