Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

RL78G13 RDK Maximum Supply Voltage

Last Updated: 06/09/2015

Question:

What is the Maximum Supply Voltage that RL78G13 RDK Can Accept?

Answer:

Do not exceed 5.5 volts on these 2 inputs. It is preferable to use a 5.0 regulated source.
  • Was this article helpful?