Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can a lead-free product be identified while it is in its packing box?

Latest Updated:04/01/2007

Question:

Can a lead-free product be identified while it is in its packing box?

Answer:

Lead-free product can be identified on the label on the packing box or reel of tape-packaged products.
Lead-free products have "Pb-Free T." shown in the upper right part of the label.
"INTP" which shows the full order code has a code, such as "-A" or "-AZ", that indicates a lead-free product.

Suitable Products