Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

In what container are operational amplifiers and comparators packed?

Latest Updated:03/01/2007

Question:

In what container are operational amplifiers and comparators packed, except in a reel or tape?

Answer:

SOP and DIP package products are supplied in magazine containers.
TSSOP products are not available as non-reel products. They are only offered in tape packing containers.

For details on magazines and tapes, refer to Packing.

(2007/03)

Suitable Products
Comparators