Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What is the difference between each orderable part number?

Latest Updated:09/02/2013

Question:

What is the difference between each orderable part number?

Answer:

Orderable part numbers are displayed on each product information page. Information such as packing is also shown for each orderable part number. The orderable part number differs with packing and RoHS compliance.
Suitable Products
Power MOSFETs for General Switching