"Any suggestions on how to get the VREF value I needed? "
Latest Updated:03/01/2005
Question:
(A/D Converter) When I create the VREF voltage using a dividing resistor, I cannot get the VREF value I need. Any suggestions ? [2005/03/01]
Answer:
Since the VREF is connected to the internal resistor, when an external dividing resistor is used, the voltage is lowered by the internal resistor. Please adjust with a variable resistor. (#104837)
Suitable Products
3803H |
3803L |
3823 |
3850A |
3858 |
38D2 |
38D5 |
7544 |
7546 |
7547 |