Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(3803L) How to find Icc for frequencies that are not included on ECT?

Latest Updated:03/01/2005

Question:

(Electrical Characteristics)   How can I find the Icc for frequencies that are not included on the Electrical Characteristics Table? [2005/03/01]

Answer:

Please refer to "3.2 Typical characteristics: Power source current characteristic example" in your user's manual.
Note that standard characteristics examples are measurement examples using standard samples; the values are provided for reference only and are not guaranteed. (#104890)
Suitable Products
3803H
3803L
3850A