Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(3803L) Is it ceramic oscillation or RC oscillation for the selection of XIN?

Latest Updated:06/09/2005

Question:

(Clock)  When using XIN as the external clock, should the oscillation mode selection bit (bit5) in the CPU mode register (003Bh) be set to ceramic/crystal oscillation or RC oscillation ? [2005/06/09]

Answer:

Set to ceramic/crystal oscillation.
Apply the external clock to XIN and leave XOUT open. Set the external clock Duty to 50%. (#105199)
Suitable Products
7544