Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(380X, 385X, 75XX) Are there ways to cut MCU's current consumption using A/D conversion?

Latest Updated:08/05/2009

Question:

(A/D Converter, Power Save)
Are there any ways to reduce the MCU's current consumption when using A/D conversion? [2009/08/05]

Answer:

The following methods are available.
Please perform A/D conversion only when sampling is necessary.
In addition, when using wait mode or stop mode, please make sure to set as below:

  • A/D input pin: Fix the A/D input pin to High or Low externally
  • Complete an A/D conversion
    (Confirm that the A/D conversion completion bit is set to 1.)

(#107427)

Suitable Products
3803H
3803L
3850A
3858
7544
7546
7547
7548
7549