Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(4286,4571) Can operation of the voltage drop detection circuit be stopped?

Latest Updated:03/04/2005

Question:

(Low Voltage Detection/LVD)   Can operation of the voltage drop detection circuit be stopped? [2005/03/04]

Answer:

The voltage drop detection circuit can be stopped by driving the VDCE pin low, or by going into power down mode without during high input without executing the SVDE instruction. (#105067)
Suitable Products
4559
455A