Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(4508) How do you enable protection in the QzROM version?

Latest Updated:05/24/2007

Question:

(QzROM)  How do you enable protection in the QzROM version? [2007/05/24]

Answer:

For QzROM programming using a programmer, use the programmer to set protection. Refer to the programmer manual for the setting method.
For MCUs that are programmed by Renesas Electronics before shipment, use the ROM option in the mask file converter (MM) to set.
However, ROM code protection cannot be enabled/disabled from a source file or a HEX file. (#106673)
Suitable Products
4286
4508
4509
4559
455A
4571