(7546,7547) Are latch and timer written to during write in and timer value read out?
Latest Updated:09/29/2006
Question:
(Timer) Are the latch and the timer simultaneously written to during write-in and the timer value read during read-out regardless of whether the timer is in operation or suspended? [2006/09/29]
Answer:
It depends on the type of timer, as detailed below:
- Timer 1 and X:
- The timer and latch are written to simultaneously and the timer count value is read.
- Timer A and B:
- The user can choose to have the value written only to the latch or to both the timer and the latch using the timer write control bit setting.
(#106383)
Suitable Products
7546 |
7547 |