Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(H8/300H Tiny) Can the empty areas of the I/O registers be used as ROM?

Latest Updated:03/26/2009

Question:

Can the empty areas of the I/O registers be used as ROM?

Answer:

The empty areas of the I/O registers cannot be used.
Suitable Products
H8/300H Tiny
H8/36109
H8/36087
H8/36077, H8/36079
H8/36064
H8/36049
H8/36037, H8/36057
H8/36014, H8/36024
H8/3694
H8/3687
H8/3672
H8/3664
H8/36912, H8/36902