Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

(H8SX) Is it possible to set φ output pin as I/O port output pin?

Latest Updated:12/25/2008

Question:

Is it possible to set φ output pin as I/O port output pin?

Answer:

No. φ output pin cannot be set as I/O port output pin. (There is no alternative settings.)
Suitable Products
H8SX/1720S (H8SX/1720, H8SX/1720S)
H8SX/1668R, H8SX/1668M
H8SX/1663
H8SX/1658R, H8SX/1658M
H8SX/1657
H8SX/1653
H8SX/1650, H8SX/1651
H8SX/1648G, H8SX/1648H
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622
H8SX/1580
H8SX/1568
H8SX/1558
H8SX/1544
H8SX/1520R