Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

After the reset release, which clock does CPU operate with?

Last Updated:12/26/2017

Question:

After the reset release, which clock does CPU operate with?

Answer:

R8C/1x Series, R8C/2x Series: 
    CPU operates with the low-speed on-chip oscillator clock divided-by-8.

R8C/3x Series, R8C/Lx, R8C/Mx Series: 
    CPU operates with the low-speed on-chip oscillator clock with no division.

Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/Lx
R8C/Mx