Are NC pins connected to any of the internal circuitry of the CPU?
Latest Updated:03/25/2009
Question:
Are NC pins connected to any of the internal circuitry of the CPU?
Answer:
No, NC pins are not connected to any of the internal circuitry of the CPU.
Suitable Products
H8/300H Tiny |
H8/36109 |
H8/36087 |
H8/36077, H8/36079 |
H8/36064 |
H8/36049 |
H8/36037, H8/36057 |
H8/36014, H8/36024 |
H8/3694 |
H8/3687 |
H8/3672 |
H8/3664 |
H8/36912, H8/36902 |