Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Are the results the same if A/D conversion is performed multiple times?

Latest Updated:02/27/2012

Question:

When A/D conversion of a certain voltage is performed multiple times with the same channel, are the results the same every time?

Answer:

When A/D conversion is performed multiple times in the same ideal environment, where the power supply voltage, VREF voltage, analog voltage, etc. are stable, the results are theoretically the same.
However, in practice, the conversion value may not be the same because the power supply voltage and analog voltage, etc. may not be in an ideal state with regard to noise etc. This is noticeable when the analog input voltage is near to the digital value of the transition point.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N