Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can I reset the MCU without supplying a clock?

Latest Updated:02/14/2006

Question:

Can I reset the MCU without supplying a clock?

Answer:

The clock is required to reset the MCU. If you don't supply a clock to the MCU, the circuit will not be reset. During reset, always apply the power supply voltage as indicated in the guaranteed operating conditions and input a stable clock.
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/1N