Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can RAM be handled as a RAM unless virtual flash emulation performed?

Latest Updated:10/29/2005

Question:

Can the internal RAM be handled as a simple RAM unless virtual flash emulation is performed?

Answer:

When not performing virtual flash emulation, the internal RAM can be handled as a RAM. It can also be used as a RAM even when using virtual flash emulation.
Suitable Products
32170, 32174
32171
32172, 32173
32176
32180
32182
32185
32186
32192
32195
32196