Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can any interrupt accepted if an INC instruction interrupt in process?

Latest Updated:02/14/2006

Question:

When an INT instruction interrupt, which is a non-maskable interrupt, is in process, can't any other interrupt be accepted?

Answer:

When an INT instruction is executed, the program branches to the INT interrupt process. In the interrupt process, although the I flag goes to the interrupt disable state ("0"), the processor interrupt priority level (IPL) is not changed. Consequently, if a maskable interrupt which has a higher priority level than the IPL is requested after the I flag is set to "1" in the interrupt process, it will be accepted. If a non-maskable interrupt is generated, it will be executed regardless of the setting of the I flag.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N