Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can clock monitor bit be used if XIN clock oscillation is stabilized?

Latest Updated:04/05/2011

Question:

Can the clock monitor bit (OCD3 bit or XINHALT bit) be used to confirm if the XIN clock oscillation is stabilized?

Answer:

No. The wait time until oscillation stabilizes should be generated in the program using the time shown in the matching evaluation provided by the oscillator manufacturer.
Suitable Products
R8C/1x
R8C/2x
R8C/3x
R8C/38A
R8C/Lx
R8C/Mx