Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can data with 257 bytes or more be placed in each chip selected area?

Latest Updated:03/08/2012

Question:

When "multiplexed bus for the entire space" is selected, can data with the size of 257 bytes or more be placed in each chip select area?

Answer:

No, it cannot. As the upper address bus works as the port when "multiplexed bus for the entire space" is selected, up to 256 bytes area are usable for each chip select.
Suitable Products
M16C/62A
M16C/62A(M16C/62T)
M16C/62M
M16C/62N
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C