Can the empty areas of the vector table be used as ROM?
Latest Updated:03/26/2009
Question:
Can the empty areas of the vector table (reserved by system or reserve) be used as ROM?
Answer:
The vector numbers reserved by the system on the vector table cannot be used. Reserve addresses, however, can be used as ROM. Unused interrupt vector addresses on the vector table can also be used.
Suitable Products
H8/300H Tiny |
H8/36109 |
H8/36087 |
H8/36077, H8/36079 |
H8/36064 |
H8/36049 |
H8/36037, H8/36057 |
H8/36014, H8/36024 |
H8/3694 |
H8/3687 |
H8/3672 |
H8/3664 |
H8/36912, H8/36902 |