Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can transmitted data be outputted when reception overrun error occurs

Latest Updated:03/16/2017

Question:

I am using a serial interface in CSIO mode. Can transmitted data be outputted normally when a reception overrun error occurs during transmission?

Answer:

Even when transmit operation is performed after an overrun error occurred while receiving data, normal transmit data is output. The data written into the SIO transmit buffer register to start the intended transmit operation.
Suitable Products
32170, 32174
32171
32172, 32173
32176
32180
32182
32185
32186
32192
32195
32196