Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can you explain further about the serial I/O specification?

Latest Updated:03/01/2005

Question:

(Serial Interface)   Regarding the serial I/O specification in which the addresses of the transmit buffer register and the receive buffer register are the same:
(1) Can data be received while a transmit is being performed?
(2) Is the shift register the same for both transmit and receive?
[2005/03/01]

Answer:

(1) Yes, data can be received while a transmit is being performed.
(2) There are separate circuits for the transmit and receive shift registers. Although the addresses in memory are the same, they each have their own buffer shift register. Accordingly, the transmit buffer register is accessed during a write and the receive buffer register is accessed during a read.

(#104794)

Suitable Products
3803H
3803L
3823
3850A
3858
38D2
38D5
7544
7546
7547
7548
7549