Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Do I have to be careful when switching from Flash to Mask version?

Latest Updated:02/27/2012

Question:

"Question" copy

Answer:

Yes, it can also be used as as a program area.
With this application in mind the data Flash area is located in the near area, and high speed memory access is possible.
Suitable Products
M32C/88
M32C/87
M32C/85
M32C/84
M16C/62A(M16C/62T)
M16C/62M
M16C/62N(M3062GF8NFP, M3062GF8NGP)
M16C/62P
M16C/63
M16C/64
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L
M16C/56
M16C/5LD
M16C/56D
M16C/5M
M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/1N