Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Do suitable products support the SPI (Serial Peripheral Interface)?

Latest Updated:02/24/2012

Question:

Do the suitable products shown below support the SPI (Serial Peripheral Interface)?

Answer:

Yes, they support the SPI.
You need to use programmable I/O ports to control the SS pin. For details, download the latest hardware manual and refer to "Special Mode 2" in the Serial Interface Chapter.
Suitable Products
M16C/62P
M16C/63
M16C/64A
M16C/64C
M16C/65
M16C/65C
M16C/6C
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/5L, M16C/56
M16C/5LD, M16C/56D
M16C/5M, M16C/57
M16C/30P
M16C/29
M16C/28
M16C/26A