Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Do you have any plans to support the block erase of M16C Flash Starter?

Latest Updated:02/14/2006

Question:

Currently, the M16C Flash Starter only supports a total erase. Do you have any plans to support the block erase?

Answer:

We don't have any plans to do this.
Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/10
R8C/11
R8C/12
R8C/13
R8C/14
R8C/15
R8C/16
R8C/17
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC
3803H
3803L
3850A
38D2
38D5
M32C/87
M32C/86
M32C/85
M32C/84
M32C/83
M16C/80
M16C/62A
M16C/62M
M16C/62N
M16C/62P
M16C/6N4, M16C/6N5
M16C/6NK, M16C/6NL, M16C/6NM, M16C/6NN
M16C/30P
M16C/29
M16C/28
M16C/26A
M16C/26
M16C/1N
M16C/6S
EV5-ASIA (R0K3306S0D011BR)
EV5-US (R0K3306S0D010BR)
SDK-PLC-EU-A (or -B for CENELEC B band)
M3A-0806