Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Does CKE0/1 bit of BRR or SCR need to be set for external clock?

Latest Updated:12/25/2008

Question:

If SCI is enabled by external clock, does CKE0/1 bit of Bit Rate Ragister (BRR) or Serial Control Register (SCR) need to be set for external clock?

Answer:

No. In case of synchronized external clock input, CKE bit of BRR or SCR doesn't need to be set for either transmit/receive operation.
Suitable Products
H8SX/1720S (H8SX/1720, H8SX/1720S)
H8SX/1668R, H8SX/1668M
H8SX/1663
H8SX/1658R, H8SX/1658M
H8SX/1657
H8SX/1653
H8SX/1650, H8SX/1651
H8SX/1648G, H8SX/1648H
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622
H8SX/1580
H8SX/1568
H8SX/1558
H8SX/1544
H8SX/1520R