Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How to get continuous serial communications using minimal CPU usage?

Latest Updated:03/23/2009

Question:

How is it possible to get continuous serial communications using minimal CPU usage ?

Answer:

"By using the SCI in conjunction with the DTC or DMAC, it will be possible to get continuous transmission or reception via a SCI.

The interrupts generated by the SCI to indicate successful data transmission / reception can be taken by the DTC to update the TDR with new data to transmit / remove data from the RDR. The DTC will clear the relevant interrupt flags so that transmission / reception can continue."

Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B