How to program FDT and E8 to do some on board programming on the QzROM?
Latest Updated:07/31/2008
Question:
(QzROM, Programmers) I am using a Flash Development Toolkit (FDT) and E8a to do some on-board programming on the QzROM version but am unable to program. Why? [2008/07/31]
Answer:
You need an IC Socket Board when on-board programming the QzROM version.
Connect an IC socket board between the E8a and user board.
Click here for more details. (#107063)
Connect an IC socket board between the E8a and user board.
Click here for more details. (#107063)
Suitable Products
3803H |
3823 |
3850A |
3858 |
38D2 |
38D5 |
7544 |
7545 |
7546 |
7547 |
7548 |
7549 |
E8a |
E8 |