Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How to set for the pull up resistance value between pins Vcc and RESET?

Latest Updated:10/31/2008

Question:

Incorrect operation occurs while using the power-on reset function. What could be causing this problem? What should I set for the pull-up resistance value between pins Vcc and RESET?

Answer:

If there is no possibility of external surge input to the RESET pin, resistance is not required between pins Vcc and RESET. For possible causes of incorrect operation, check the following:

  1. Is the power rise gradient of the MCU Vcc pin within the specifications of the Electrical Characteristics?
  2. When the power rises, does the RESET pin always maintain the voltage of 0.8 × Vcc or above?
  3. When using the power-on reset function, voltage monitor reset must be also used. Is the voltage monitor reset function is enabled?

 

Suitable Products
R8C/18
R8C/19
R8C/1A
R8C/1B
R8C/20
R8C/21
R8C/22
R8C/23
R8C/24
R8C/25
R8C/26
R8C/27
R8C/28
R8C/29
R8C/2A
R8C/2B
R8C/2C
R8C/2D
R8C/2E
R8C/2F
R8C/2G
R8C/2H
R8C/2J
R8C/2K
R8C/2L
R8C/32C
R8C/33C
R8C/34C
R8C/35C
R8C/36C
R8C/38C
R8C/3GC
R8C/3JC
R8C/32D
R8C/33D
R8C/35D
R8C/3GD
R8C/33T
R8C/38A
R8C/34E, R8C/34F, R8C/34G, R8C/34H
R8C/36E, R8C/36F, R8C/36G, R8C/36H
R8C/38E, R8C/38F, R8C/38G, R8C/38H
R8C/L35C
R8C/L36C
R8C/L38C
R8C/L3AC