Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

In H form, can operation of voltage drop detection circuit be stopped?

Latest Updated:01/16/2006

Question:

(Low Voltage Detection/LVD)   In the H version, can operation of the voltage drop detection circuit be stopped? [2006/01/16]

Answer:

The voltage drop detection circuit cannot be stopped during MCU operation. It can be stopped in RAM back-up mode. It can also be operated by executing the SVDE instruction in RAM back-up mode. (#105589)
Suitable Products
4508
4509