Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Is it needed to integrate the serial I/O in CPU reprogramming mode?

Latest Updated:03/01/2005

Question:

(Flash Memory)   When data is written to the Flash memory through a serial I/O, is it necessary to integrate the serial I/O control program in the CPU reprogramming mode control program? [2005/03/01]

Answer:

Yes. In addition to integrating the serial I/O control program, the user also needs to initialize the ports, etc., disable interrupts, write to the watchdog timer, etc.
Suitable Products
3803H
3803L
3850A
38D2