Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Power Save: Return conditions for key-on wakeup, edge or level?

Latest Updated:04/26/2005

Question:

(Power Save)  What are the return conditions for key-on wakeup, edge or level? [2005/04/26]

Answer:

The MCU returns by level. For this reason, if the key-on wakeup enable pins are in the return condition state when the MCU switches to RAM back-up mode, the MCU will return immediately.
Please refer to the datasheet for more details concerning the return conditions. (#105025)
Suitable Products
4286