Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Setting PSi Register using port as input pin of on-chip peripherals?

Latest Updated:02/14/2006

Question:

How should I set PSi Register when I use the port as the input pin of the on-chip peripherals?

Answer:

Set the register to "0" (I/O port).
Suitable Products
M32C/8A
M32C/88
M32C/87
M32C/85
M32C/84
M32C/83
M32C/80