Should data be set from b15 or b0 when using SSU to perform 9-15 bit data transfer?
Last Updated:12/26/2017
Question:
When using the synchronous serial communication unit (SSU) to perform 9- to 15-bit data transfer, should the data be allocated from b15, or b0?
Answer:
Allocate the data from b0. Write 2FFh in 16-bit units when transmitting 2FFH (10-bit data).
Suitable Products
R8C/3x |
R8C/5x |
R8C/Lx |
R8C/Mx |