Skip to main content
Renesas Electronics America - Knowledgebase

What's the difference between the IE-780078-NS-EM1 and the D78F0078?

Latest Updated:12/01/2011


Are there differences in the microcontroller functions (existence of internal pull-up resistor selection, etc.) between the IE-780078-NS-EM1 and the D78F0078?


Regarding the internal pull-up resistor, the P30 to P33 mask option resistors are emulated with the ICE, but these resistors as mask options and are not included in the flash version.
However, there are no differences regarding pull-up resistors connected by software.
The differences between the device and ICE are described in the IE-780078-NS-EM1 manual.
There are differences in the clock oscillator and I/O port configuration.
Suitable Products
78K Family