Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What's the differences of three mode's for memory in 0.18 μm version?

Latest Updated:03/06/2008

Question:

What's the difference between boot mode, user boot mode, and user program mode for flash memory in the 0.18 μm process version?

Answer:

Boot mode is used for transmitting control commands and write data from a host via SCI or USB, and programming/erasing such commands or data in the user mat and user boot mat. User boot mode is used for executing programs from the user boot area (programs must be preprogrammed into the user boot area during boot mode). User program mode is used for programming/erasing to the user mat using programming/erase control programming created in advance by the MCU's on-chip programming/erase program. In addition, please note that you cannot program/erase to the user boot mat in user program mode.
Suitable Products
H8S/2378, 2378R
H8S/2368
H8S/2189R
H8S/2172
H8S/2168
H8S/2116
H8S/2114R
H8SX/1720S (H8SX/1720, H8SX/1720S)
H8SX/1668R, H8SX/1668M
H8SX/1663
H8SX/1658R, H8SX/1658M
H8SX/1657
H8SX/1653
H8SX/1650, H8SX/1651
H8SX/1648A, H8SX/1648L
H8SX/1638, H8SX/1638L
H8SX/1622
H8SX/1580
H8SX/1568
H8SX/1558
H8SX/1544
H8SX/1520R