Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What are the Hardware differences and Instruction set differences?

Latest Updated:03/23/2009

Question:

The H8S series has two CPU cores. What are the Hardware differences and the Instruction set differences?

Answer:

"Hardware Differences are : H8S/2000No MAC Unit  and H8S/2600H/W MAC Unit

Instruction set differences are : The H8S/2600 has 4 additional instructions to untilise the MAC unit (MAC,CLRMAC,LDMAC and STMAC).

MULXU and MULXS take fewer cyclesto execute on H8S/2600."

Suitable Products
H8S/2668
H8S/2655
H8S/2643
H8S/2633
H8S/2628
H8S/2615
H8S/2612
H8S/2437
H8S/2368
H8S/2398, 2357
H8S/2355
H8S/2350
H8S/2345
H8S/2282, 2280
H8S/2276
H8S/2258, 2239, 2238, 2237, 2227
H8S/2245
H8S/2215
H8S/2214
H8S/2199R
H8S/2194
H8S/2172
H8S/2168
H8S/2158
H8S/2140B
H8S/2114R
H8S/2111B
H8S/2110B