Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What can be done to avoid performance loss from off-chip memory?

Latest Updated:03/18/2009

Question:

Is there anything that can be done against the performance loss when executing from off-chip memory ?

Answer:

Most software spends 90% of its time in only a small number of small inner loops. These could be copied from off-chip memory into on-chip RAM after reset and then be executed there. This way the performance loss may be almost fully compensated fo. Also some derivatives have bus controllers that implement countermeasures against the performance loss e.g. write buffer and burst mode
Suitable Products
H8S Family