Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What does the N mean in the H8/3877N part name ?

Latest Updated:03/18/2009

Question:

What does the N mean in the H8/3877N part name ?

Answer:

The N mean in the H8/3877N part name denotes an H8/3877 devices that does not have the on-chip LCD driver function. The pins normally used by the LCD display driver can be used as normal digital I/O pins.
Suitable Products
H8/300L